Změna jazyka :

New test standard for cables in moving applications guarantees reliability in maritime use
igus® GmbH and the DNV classification society have jointly developed a new test standard so that cables for moving applications can be used on ships and in offshore applications without complex and cost-intensive special approvals, and have now awarded a total of 387 chainflex® cables from igus® with a type approval for permanently moving cables in e-chain®. This makes them the world's first cables specifically for energy chain applications to receive this certificate.
In order to supply safe and suitable products for this special area of application, igus® GmbH from Cologne has developed a new test procedure in cooperation with the DNV classification society and had its chainflex® cable certified.
Development of new test procedure necessary
Classification societies, such as DNV, typically issue approvals that adhere to international standards. In many cases, these refer to special specifications in terms of fire behaviour or other requirements, particularly for materials.
The specialised knowledge of the two companies over a long certification period of more than three years with the most diverse areas of investigation has led to the first-ever certification of cables for use in the energy chain on ships and offshore applications.

What challenges and what advantages do automation and digitisation present for the maritime industry? How can companies meet the strict test criteria to have components certified by competent institutions such as DNV GL? What opportunities arise for suppliers, plant constructors, and operators of drilling platforms and ships from the use of certified components such as cables?
control cable
chainflex® cable CF9.UL and CF10.UL (PDF), CF77.UL.D and CF78.UL (PDF)
bus cable
chainflex® cable CFBUS.PUR(PDF), CFBUS (PDF), CFBUS Ethernet (PDF), CFBUS.PUR Ethernet (PDF)
Fibre Optic Cable (Fibre Optic Cable)
chainflex® cable CFLG.LB.PUR (PDF)
measuring system cable and data cable
chainflex® cable CF111.D and CF113.D (PDF)
CF112 and CF211.PUR (PDF) CF240.PUR (PDF)
motor cable and servo cable
chainflex® cable CF300.UL.D, CF310.UL and CFPE (PDF), CF27.D (PDF) CF34.UL.D and CF35.UL (PDF)

NEK 606 is a Norwegian standard for cables in offshore applications. 301 chainflex® cables fulfil the requirements of the NEK 606 standard.
Control cables
data cables
Measuring system cables
servo cables

The newest generation of the P4.1 rol e-chain with a smart sensor
The roller energy chain has been the tried-and-tested energy supply for long travels for about 20 years. Besides the successful design that distinguishes all of our linear energy chain systems, stainless steel rollers are added, which upgrade the energy chain to energy supply for heavy-duty applications. As the energy chain rolls and does not glide, it runs quietly and with low vibration. Wear is significantly lower than for designs without rollers, and the power needed for movement is also lower by as much as 57%.

Largest laboratory for moving cables. 25 years of experience. 3,800 m² test area
Osobne:
Pondelí až pátek od 7:00 do 16:00.
Online:
24h